PROFINET.USEMODULECFG
Description
This command controls where the drive obtains the telegram configuration. When set to 1 (default), the drive uses the telegram setting from the module configuration in the PROFINET master. When set to 0, the drive uses the telegram setting specified in AXIS#.PROFINET.TELEGRAMID (P922).
| Value | Description |
|---|---|
| 0 |
Drive uses the telegram specified from AXIS#.PROFINET.TELEGRAMID (P922) |
|
1 (default) |
Drive uses telegram configuration from the sub-module configuration in the PROFINET master. |
-
- When this keyword is set to 1 (use PLC configuration), AXIS#.PROFINET.TELEGRAMID and AXIS#.PROFINET.​SUPPTELEGRAMID keywords are set to read only.
For more information, see Telegram Mappings.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-04-05-000 |
General Information
| Type | Read/Write |
| Units |
N/A |
| Range | 0 to 1 |
| Default Value | 1 (Use sub-module configuration from PLC) |
| Data Type | Integer |
| Stored in Non-Volatile Memory | Yes |
Variants Supported
PROFINET drives: AKD2G-SPP
Industrial Ethernet Information
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
PROFINET.USEMODULECFG |
5211 |
Unsigned8 |
Read/Write |
- |